Technical FAQs

Ask a Question

Which S-Flex SFD212 drives are stocked and what is the lead time on ordering non stocked units?

Issue:
Which S-Flex SFD212 drives are stocked and what is the lead time on ordering non stocked units?

Product Line:
Altivar ATV212 SFD212

Environment:
All

Cause:
They want to what is the lead time on adding the X07 line reactor mod on the SFD212 enclosed drives.

Resolution:
Most of the 460VAC SFD212 S-Flex drives are stocked with Modifications B07 (Line contactor)  and D07 (Door mounted HMI) only.
If you need to add any other modifications or voltages you will need to build the unit up on as a special on product selector.
You will need to contact customer service at 1-888-778 2733 option 3 to get lead times.

Was this helpful?
What can we do to improve the information ?