Technical FAQs

Ask a Question

Do we sell the ATS46 cable to connect between the remote keypad and the ATS46 soft starter?

Issue:
Do we sell the ATS46 cable to connect between the remote keypad and the ATS46 soft starter?

Product Line:
Altistart ATS46

Environment:
All

Cause:
They need the remote cable that mounts between the remote keypad and the Soft starter

Resolution:
We don't sell the cable alone.  The cable comes with the remote mounting kit VW3-G46103 however this kit is obsolete and no longer available.
http://download.schneider-electric.com/files?p_File_Id=2930103&p_File_Name=1494125.pdf

Was this helpful?
What can we do to improve the information ?