Technical FAQs

Ask a Question

What is the replacement part number for the firing board for the ATS48D75Y soft starter?

Issue:
What is the replacement part number for the firing board for the ATS48D75Y soft starter?

Product Line:
Altistart ATS48

Environment:
All

Cause:
SCR firing board needs to be replaced

Resolution:
VX5G48D75Y is the replacement power board which has the firing board on it.
Ref the ATS48 soft starter troubleshooting manual for more information 30072-451-28

Was this helpful?
What can we do to improve the information ?