Technical FAQs

Ask a Question

What is the wire termination data for a size 5, Nema starter such as 8536 type SG?

Issue:
What is the wire termination data for a size 5, Nema starter such as 8536 type SG?

Product Line:
NEMA starters

Environment:
8536, 8736 Size 5 starters

Cause:
To determine wire size needed.

Resolution:
Power Terminals will accept #4 - 500 kcmil, control terminals will accept #16- 12
 
Was this helpful?
What can we do to improve the information ?