Technical FAQs

Ask a Question

Can I get a drawing that shows the use of a larger power supply to power up my Schneider Electric Low Voltage Occupancy sensors?

Issue:
Customer does not want to have multiple SLSPP1277 power pack installed and would prefer to have a single power supply mounted in a panel.

Note: As of March 1, 2015 all US Lighting Control products (EXCEPT Powerlink and MVP panels) will enter their obsolescence phase and will no longer be purchasable for new orders. Management of the Prosumer Business has made a strategic decision to stop the Lighting Control initiative and concentrate our effort in new businesses with higher growth potential – Connected Home, Building Control in small buildings, and Electric Vehicle solutions.

Product Line:
Schneider Electric Occupancy Sensor Lighting Control products

Environment:
Schneider Electric Low Voltage Occupancy Sensors

Cause:
SLSPP1277 power packs source 24 Vdc at 100mA. Application is multiple ceiling mount low voltage sensors controlling Aux Relay SLSSP24.

Resolution:
Use a larger panel mount power supply to power up multiple sensors (see drawing)


http://static.schneider-electric.us/docs/Power%20Management/Lighting%20Control/Square%20D%20Occupancy%20Sensor%20Products/CAD%20DRAWINGS/WIRING%20DIAGRAMS%20Low%20Voltage/63249-600-47.pdf
Was this helpful?
What can we do to improve the information ?