Technical FAQs

Ask a Question

Wiser thermostat buttons do not change temperature setting

Issue:
Wiser Thermostat will not accept input from button pushes.

Product Line:
PTLRC - LIGHT AND ROOM CONTROL

Environment:
Residential HVAC Systems

Cause:
Wiser Thermostat EER58000 has the ability to lock out front panel usage.

Resolution:
The temperature settings on the EER58000 thermostat can be adjusted manually if the buttons have not been locked. 
This feature is activated by pressing the Up and Down arrows at the same time and locks out all button functions.
Wiser EER58000 Panel View

The Button Lock Symbol will appear on the display when active (and disappear when de-activated) as shown circled in orange below;
Wiser Screen with Button Lock Symbol


For more information on Wiser Products please visit here.
Was this helpful?
What can we do to improve the information ?