Technical FAQs

Ask a Question

What are the UL electrical ratings for NSYTRP24 Linergy Terminal block?

Issue:
Needs to find the UL and CSA certification ratings for terminal block NSYTRP24.

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Linergy TR NSYTRP24, NSYTRP24BL

Cause:
To clarify the difference between the new line of terminal blocks compared to the old AB1 terminal blocks.

Resolution:
600V,20AMPS, All certifications for this terminal block is found on page 61 in the LINERGY CATALOG 9080CT1301
 

Was this helpful?
What can we do to improve the information ?