Technical FAQs

Ask a Question

Where can I find information on terminal block NSYTRP23?

Issue:
Need to locate certifications and electrical specifications for the NSYTRP23 terminal block.

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Linergy TR NSYTRP23,NSYTRP23BL, NSYTRP23AR

Cause:
To clarify the difference between the new line of terminal blocks compared to the old AB1 terminal blocks.

Resolution:
All of the certifications and electrical specifications for this terminal block is found on page 60 in the LINERGY CATALOG 9080CT1301

Was this helpful?
What can we do to improve the information ?