Technical FAQs

Ask a Question

What are the dimensions for the NSYTRP22 Linergy terminal block?

Issue:
Needs dimensions for terminal block NSYTRP22

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Linergy TR NSYTRP22, NSYTRP22BL, NSYTRP22AR 

Cause:
To help design the layout out on a panel for many terminal blocks

Resolution:
The measurements are 48.5 L, 36.5 H, 5.2 W, All information for this terminal block is found on page 60 in the LINERGY CATALOG 9080CT1301
 

 

Was this helpful?
What can we do to improve the information ?