Technical FAQs

Ask a Question

In the M-Flex enclosures, do we have an ATV61 drive that is rated at 300hp?

Issue:
In the M-Flex enclosures, do we have an ATV61 drive that is rated at 300hp?

Product Line:
ATV61

Environment:
All serial numbers for ATV61

Cause:
N/A

Resolution:
We do not have a 300hp ATV61 open style drive.  We do have a 350hp open style drive.  When selecting an M-Flex for a variable torque application there is an option for 300hp.  However, what comes inside the unit is an ATV61HC22N4 which is rated at 350hp at 460VAC. 
 
Was this helpful?
What can we do to improve the information ?