Technical FAQs

Ask a Question

Can you use 120vac to start and stop the ATS48 soft starters?

Issue:
Can you use 120vac to start and stop the ATS48 soft starters?

Product Line:
Altistart ATS48

Environment:
All

Cause:
Needs a option card to allow 120vac start stop control

Resolution:
There is not an option to control the ATS48 soft starter with 120vac control voltage.  In this case you will need to add an interposing relay.

Was this helpful?
What can we do to improve the information ?