Technical FAQs

Ask a Question

PK1MB Retaining Kit for NQ/NQOD Panelboards

Can the PK1MB main breaker retaining kit be used for a backfed main breaker for the NQ or NQOD line of panelboards?

Product Line:
NQ/NQOD panelboards sold and supported in the USA>


Is a retaining kit required for a backfed main breaker in the NQ/NQOD panelboards?

No, the PK1MB is strictly for use in load centers and will not work in a panelboard application.  Both the NQ and NQOD panelboards accept QOB bolt on branch circuit breakers which do not require
a retaining kit.  

Was this helpful?
What can we do to improve the information ?