Technical FAQs

Ask a Question

Is the EZM3600CB available with alternate trip settings?

Issue:
Application

Product Line:
EZM

Environment:
Main Breaker

Cause:
Selection

Resolution:
Yes, altenate trip settings are available: Order EZM3600CB500 for 500A trip; EZM3600CB450 for 450A trip; EZM3600CB400 for 400A trip.
Was this helpful?
What can we do to improve the information ?