Technical FAQs

Ask a Question

How can you assign an logic input to do a fault reset on the ATV71/61 drives?

Issue:
How can you assign an logic input to do a fault reset on the ATV71/61 drives?

Product line: 
ATV61/ATV71

Environment:    
All serial number

Cause:
None

Resolution:
To assign fault reset on the ATV61/71 do the following
Main Menu Press enter
Drive Menu Press enter
Fault Management Menu Press enter
Fault reset submenu press enter
Fault reset = select a logic input LIX to be assigned to an input that will be your fault reset.

Was this helpful?
What can we do to improve the information ?