Technical FAQs

Ask a Question

Is the HOM4080L225PC, a main lugs load center, convertible to be a main breaker load center?

Issue:
Product Feature

Product Line:
HOMELINE Load Center

Environment:
Main Lugs

Cause:
Convert to Main Breaker

Resolution:
Yes, this is a convertible main load center which uses the QOM2-VH frame of main breaker. To convert to a 225A main breaker, order QOM2225VH.
 

Was this helpful?
What can we do to improve the information ?