Technical FAQs

Ask a Question

Is external overload required with an ATV61 drive?

Issue:
Is external overload protection required with an ATV61 drive?

Product Line:
ATV61

Environment:
All

Cause:
None

Resolution:
The drive provides standard overload protection , in most cases.
If using multiple motors on a single drive external overload protection is required for each motor.
Was this helpful?
What can we do to improve the information ?