Technical FAQs

Ask a Question

Can the main breaker in EZM31600GCBC be adjusted down to 1400A?

Issue:
Adjustable trip range

Product Line:
EZM Main Breaker

Environment:
1600A Main Breaker

Cause:
Different long time trip setting required

Resolution:
The RGF36160U31A main breaker can be adjusted, but has an A rating plug with .80 and .90 mulitpliers, which would adjust the 1600A setting down to 1280A or 1440A as the closest values to 1400A. If the A rating plug was replaced with a B rating plug, part number S48819, a trip setting of 1408A could be achieved by setting the B rating plug to the .88 multiplier.  
Was this helpful?
What can we do to improve the information ?