Technical FAQs

Ask a Question

What is option E414 on the M-Flex enclosed enclosed drive?

What is option E414 on the M-Flex ​ enclosed Product?

Issue:

What is option E414 on the M-Flex enclosed Product

Product Line:
8839 MFD

Environment:
All models

Cause:
None

Resolution:
The Mod E414 on the MFLEX enclosed unit is the 3% load reactor

Keywords:
Mod modification options enclosure enclosed 8839 addition load reactor E414
 
Was this helpful?
What can we do to improve the information ?