Technical FAQs

Ask a Question

What is the part number for an open style or NEMA 1 line reactor for a 1 hp 480vac variable frequency drive?

Issue:
What is the part number for an open style or NEMA 1 line reactor for a 1 hp 480vac variable frequency drive?

Product Line:
ATV312, ATV61, ATV71, ATV32,

Environment:
1 hp, 480vac

Cause:
None

Resolution:
The 5% line reactor for a variable frequency driver rated for 1 hp, 480vac is RL00202 open type and RL00212 is the NEMA 1 type

Was this helpful?
What can we do to improve the information ?