Technical FAQs

Ask a Question

ATV61 Apogee FLN P1. Where do I determine drive fault status?

Issue:
ATV61 Apogee FLN P1.  Where do I determine drive fault status?

Product Line:
ATV61 drive equipped with VW3A3314 Apogee FLN P1 Card

Environment:
All ATV61 models and serial numbers equipped with VW3A3314 Apogee FLN P1 Card.

Cause:
Customer is unsure what object to monitor over the network to determine if the drive is in a faulted condition.

Resolution:
Bit 3 of Object 93 is used to indicate the ETA status of the drive.  Monitor bit 3 of object 93 to determine if the drive is or is not in a faulted state.

 
Was this helpful?
What can we do to improve the information ?