Technical FAQs

Ask a Question

What is the dissipated watts loss for the ATV61 drives without a DC choke installed?

Issue:
What is the dissipated watts loss for the ATV61 drives without a DC choke installed?
 
Product line:
ATV61, High HP. 
 
Environment:
All serial numbers
 
Cause:
Installation manual only shows with the DC choke installed
 
Resolution:
Drive without Choke      Losses in Watts
ATV61HD90N4D           2210
ATV61HC11N4D           2810
ATV61HC13N4D           3330
ATV61HC16N4D           3710
ATV61HC22N4D           5010
ATV61HC25N4D           5890
ATV61HC31N4D           7250
ATV61HC40N4D           8810
ATV61HC50N4D           11150
ATV61HC63N4D           13830
Was this helpful?
What can we do to improve the information ?