Technical FAQs

Ask a Question

Can the unused socket area on a EZM312225 be energized to make the 2 tenant device into a 3 tenant device?

Issue:
Application

Product Line:
EZM

Environment:
2 gang devices

Cause:
Conversion

Resolution:
No, the 2 meter device cannot be converted into a 3 meter device. Consider replacing with a EZM313225.
Was this helpful?
What can we do to improve the information ?