Technical FAQs

Ask a Question

What can I use to condition the line side of the ATV61 drive?

Issue:
High line supply

Product Line:
ATV61, ATV71, ATV312, ATV12, ATV32

Environment:
All model numbers and serial numbers

Cause:
Line voltage is high

Resolution:
One recommendation is to use a line reactor.  This is attached to the line supply voltage ahead of the VFD.

Was this helpful?
What can we do to improve the information ?