Technical FAQs

Ask a Question

There are no illuminated indicator lights on the Wiser Large Load Controller

Issue:
There are no illuminated indicator lights on the Wiser Large Load Controller.  Large Load Controller (LLC) is not working.

Product Line:
Wiser Home Management System  
EER260LLCR

Environment:
Residential Home

Cause:
The most likely cause no indicator lights on the LLC is incorrect wiring / installation.

Resolution:
Verify that the device is installed and wired correctly per the installation instructions.  As shown in the instructions, incoming power 240 or 120 VAC is terminated on the lugs at the top of the device.   Then the Black and Blue wires from the control circuit board are also landed under these same incoming power lugs.  The White wire is not used in a 240V application.  

In a 120 V application. use the Black and White wires from the control board.  Do not use the Blue wire.

Failure to use the correct power wires of the circuit board depending on the application may result in permanent damage of the device.

Instruction Bulletin of the Large Load Controller is attached.
Was this helpful?
What can we do to improve the information ?