Technical FAQs

Ask a Question

What is the size of a QMJ364T load side lug?

 
 
 

Issue:
Switch Loadside Lug size

Product Line:
Panelboards

Environment:
QMB/QMJ

Cause:
Wire termination

Resolution:

The standard mechanical or compression lug is good for one #6- 300kcmil  Al or Cu


 

 
Was this helpful?
What can we do to improve the information ?