Technical FAQs

Ask a Question

Connection piece between shaft and LK4 disconnect switch

Issue:
Does plastic clip which attaches shaft to LK4JU3CN/LK4GU3CN/LK4DU3CN come with switch or shaft?

Product Line:
LK4JU3CN
LK4GU3CN
LK4DU3CN

Environment:
US product

Cause:
Instruction bulletin 30072-454-11 is unclear as to origin of connection piece.

Resolution:
This plastic piece is included with shaft kit LK4AE12CN only.

Was this helpful?
What can we do to improve the information ?