Technical FAQs

Ask a Question

What is the internal cooling fan kit part number ATV58HU90M2, ATV58HD12M2, ATV58HD12N4, ATV58HD16N4 and ATV58HD23N4 drives?

Issue:
What is the internal cooling fan kit part number ATV58HU90M2, ATV58HD12M2, ATV58HD12N4, ATV58HD16N4 and ATV58HD23N4 drives?

Product Line:
Altivar ATV45 frame sizes 4 and 5

Environment:
All

Cause:
Needs the internal cooling fan kit part number.

Resolution:

VZ3V58245U kit contains
Qty 6 M4 X 35 screws
Qty 3 60 mm cooling fans.
 

 

 

 

Was this helpful?
What can we do to improve the information ?