Technical FAQs

Ask a Question

Can you run the ATV12H037F1 drive with a motor that will pull 2.9 amps FLA?

Issue:
Can you run the ATV12H037F1 drive with a motor that will pull 2.9 amps FLA?

Product Line:
Altivar ATV12

Environment:
All

Cause:
Needs to run the drive continuous at 2.9 amps but the drive is only rated for 2.4 amps.

Resolution:
2.4 amps is the max continuous current rating for this drive.  It does have a max transient current rating for 60 seconds at 3.6 amps but it does not allow for continuous current.

Was this helpful?
What can we do to improve the information ?