Technical FAQs

Ask a Question

Is there a guard for the 22 mm non trigger action emergency stop operators?

Issue:
Need to guard a 22 mm push button that is not trigger action, such as the XB4BT42, XB4BS542, XB4BS142, XB5AT42, XB5AT542, and XB5AS142, there are not listed guards for these.

Product Line:
22 mm XB4 and XB5 emergency stop push buttons

Environment:
22 mm emergency stop push buttons

Cause:
Need to guard a 22 mm emergency stop push button that is not trigger action
 
Resolution:
We can use the standard metal guards that we use for the trigger action emergency stops.
Because the trigger action emergency stop is 5 mm taller than the non-trigger action devices the padlock function will not work but they can still be used to guard the emergency stop operator.
A ZBZ1600 can be used for the chromium plated guard, ZBZ1602 for a black guard, ZBZ1604 for red, ZBZ1605 for yellow, and ZBZ1606 for blue.



Was this helpful?
What can we do to improve the information ?