Technical FAQs

Ask a Question

Are any Altivar drives Lonmark certified?

Issue:
Are any Altivar drives Lonmark certified?

Product Line:
Altivar 212 and Altivar 61 series.

Environment:
All models, All serial numbers.

Cause:
Customer needs the LonMark certification sheet for Altivar drives.

Answer:
The ATV212 and ATV61 series drives are Lonmark certified.  The certification pages can be found in the below links.

ATV212:
http://www.lonmark.org/certifications/device_certification/product_catalog/product_detail?ProductID=1041

ATV61:
http://www.lonmark.org/certifications/device_certification/product_catalog/product_detail?ProductID=830
Was this helpful?
What can we do to improve the information ?