Technical FAQs

Ask a Question

Do we offer a 1.5KW drive that will work on 115 VAC 1 phase input 230 VAC 3 phase output?

Issue:
Do we offer a 1.5KW drive that will work on 115 VAC 1 phase input 230 VAC 3 phase output?

Product Line:
Altivar ATV12

Environment:
All

Cause:
Drives selection for special application.

Resolution:
No The only application offering we have for 115 VAC  1 phase input 3 phase 230 VAC output are

ATV12H018F1= .1/4 HP or 0.18KW 
ATV12H037F1= 1/2HP or 0.37KW
ATV12H075F1= 1HP or 0,75KW

we do not offer this application over 1HP.

Was this helpful?
What can we do to improve the information ?