Technical FAQs

Ask a Question

There is only one phase light illuminated on Jetun Wiser Power Monitor. Data is not correct.

Issue:
There is only one phase light illuminated on Jetun Wiser Power Monitor.  Data is not correct.

Product Line:
Wiser Home Management System
WISERJLPM200

Environment:
Residential Home
Wiser System

Cause:

The electrical contractor only powered the Power Monitor with one phase of the 240/120 power.   Wired in this manner, the electronics of the Power Monitor device do operate.  The Zigbee radio circuitry does work.   But the Power Monitor will not measure both phases of the 240/120 electrical circuit.  

Resolution:
Electrician must supply voltage from a 2-pole breaker ot the Wiser Power Monitor.  Wire Phase A to the Black lead in the Power Monitor and Phase B to Red Lead.   See Power Meter Instruction Bulletin attached.
Was this helpful?
What can we do to improve the information ?