Technical FAQs

Ask a Question

Is there an option for adding a input line reactor on the 115 VAC ATV12.......F1 drives?

Issue:
Is there an option for adding a input line reactor on the 115 VAC  ATV12.......F1 drives?

Product Line:
Altivar ATV12 with suffix F1 only

Environment:
All

Cause:
Do we offer an input line reactor for the 115 VAC input ATV12 Drive?

Resolution:
No there is no option for adding a 115V line reactor.

Was this helpful?
What can we do to improve the information ?