Technical FAQs

Ask a Question

What is the part number of the recommended shorting contactor for the ATS48C66Y Soft Starter?

Issue:
What is the part number of the recommended shorting contactor for the ATS48C66Y Soft Starter?

Product Line:
ATS48 soft starters

Environment:
ATS48C66Y part number only.  All serial numbers.

Cause:
Customer purchases the starter as an individual component and wants to install a shorting contactor also.

Resolution:
The part number of the recommended shorting contactor for the ATS48C66Y is LC1F630.  Note that this is an incomplete part number, the remaining 2 digits of the part number indicate the voltage of the contactor coil.  This contactor is available in several different coil voltage ranges.  Please contact your local Schneider Electric distributor for assistance selecting the correct coil to match your application. 
Was this helpful?
What can we do to improve the information ?