Technical FAQs

Ask a Question

9001K and SK Gasketing

Issue:
Do the standard 9001K and SK selector switches come with gasket, part number  3105406401?

Product Line:
30MM standard selector switch knobs

Environment:
Installation 

Cause:
3105406401 washer/gasket is listed as separate part number in Digest 176, but it is not clear if it comes with selector switch knob.

Resolution:
Washer/gasket 3105406401 comes standard with the 9001K and SK selector switches. Four gaskets are included with each operator,  useage is dependent on panel thickness
and type of legend plate used.

Was this helpful?
What can we do to improve the information ?