Technical FAQs

Ask a Question

Can the neutral lug provided on the EZMK312400 be changed to a lug that will accept up to (2) 500 kcmil neutral conductors?

Issue:
Optional lug

Product Line:
EZM

Environment:
EZM 400A Branch

Cause:
Wires to be used exceed the factory installed lugs

Resolution:
Yes, the standard lug could be replaced with the lug provided in lug kit MMLK500. The lug wire range will be (2) 3/0 AWG - 500 KCMIL. There are three lugs provided in this kit.
Was this helpful?
What can we do to improve the information ?