Technical FAQs

Ask a Question

How can you set up the ATV31 and ATV312 to display motor current on the main display?

Issue:
How can you set up the ATV31 and ATV312 to display motor current on the main display?

Product Line:
Altivar ATV312

Environment:
All

Cause:
Needs to display motor current not output frequency.

Resolution:
Programming
Enter arrow down to SUP menu  Enter
Arrow down to the LCR menu Enter and Enter again (Twice) to save the display value to come up again after you power cycle the Drive.
 

Was this helpful?
What can we do to improve the information ?