Technical FAQs

Ask a Question

In Unity Pro, how can I set a table of EBOOLs to 0?

Issue
Need a way of resetting multiple EBOOLS to 0 

Product Line
M340 

Environment
NA
 
Cause
 NA
 
Resolution
The MOVE_DINT_AREBOOL block will allow you to reset up to 32 EBOOLs at one time.
Was this helpful?
What can we do to improve the information ?