Technical FAQs

Ask a Question

Will the QO32M100VP accept QO tandem breakers or QOT tandem breakers?

Issue:
Application

Product Line:
QO Load Center

Environment:
QO32M100VP

Cause:
Selection

Resolution:
No, the QO132M100C load center that is provided with the QO32M100VP Value Pack will accept only QO full size circuit breakers.
Was this helpful?
What can we do to improve the information ?