Technical FAQs

Ask a Question

HL4IMA20C and Replacement Module

Issue:
What is the replacement A, B and C phase module for HL4IMA20C, 200kA, 277/480V, 3PH, 4W, with ground, high resistance ground TVSS module?

Product Line:
TVSS units and modules sold and supported in the USA.

Environment:
Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can be replaced or the entire unit must be replaced.

Cause:
Maintenance

Resolution:
Replacement module for  A, B or C phase is MA5IMA20 (one module for each phase).

Was this helpful?
What can we do to improve the information ?