Technical FAQs

Ask a Question

HL4IMA12C and Replacement Module.

Issue:
What is the replacement A, B and C phase modules for HL4IMA12C, 120kA, 277/480V, 3PH, 4W, with ground wye TVSS module ?

Product Line:
TVSS units and modules sold and supported in the USA.

Environment:
Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can be replaced or the entire unit must be replaced.

Cause:
Maintenance

Resolution:
Replacement module for  A, B or C phase is MA4IMA12 (one module for each phase).
 
Was this helpful?
What can we do to improve the information ?