Technical FAQs

Ask a Question

HL3IMA24C and Replacement Module.

What is the replacement A, B and C phase modules for the HL3IMA24C, 240kA, 120/240V, 3PH, 4W, high leg delta TVSS module?

Product Line:
TVSS units and modules sold and supported in the USA.

Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can be replaced or the entire unit must be replaced.


Replacement A phase module is MA1IMA24, B phase module is MA3IMA24, C phase module is MA1IMA24.

Was this helpful?
What can we do to improve the information ?