Technical FAQs

Ask a Question

HL3IMA16C and Replacement Module

Issue:
What is the replacement A, B and C phase module for HL3IMA16C, 160kA, 120/240V, 3P, 4W, high leg delta?

Product Line:
TVSS units and modules sold and supported in the USA.

Environment:
Generally, when the TVSS unit is inoperative, it is necessary to determine if a module can be replaced or the entire unit must be replaced.

Cause:
Maintenance

Resolution:
Replacement A module is MA1IMA16, B module is MA3IMA16, C module is MA1IMA16.

Was this helpful?
What can we do to improve the information ?