Technical FAQs

Ask a Question

HL3IMA12C and Replacement Module.

Issue:
What is the replacement A, B, and C phase module for HL3IMA12C, 120kA, 120/240V, 3PH, 4W, high leg delta?

Product Line:
TVSS units and modules sold and supported in the USA.

Environment:
Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can be replaced or the entire unit must be replaced.

Cause:
Maintenance

Resolution:
Replacement A module is MA1IMA12, B module is MA3IMA12, C module is MA1IMA12.

Was this helpful?
What can we do to improve the information ?