Technical FAQs

Ask a Question

HL2IMA16C and Replacement Module

Issue:
What is the replacement A ,B and C phase modules for the HL2IMA16C, 160kA,  120/208V, 3 phase, 4 wire TVSS unit?

Product Line:
TVSS, Surgelogic

Environment:
TVSS units sold and supported in the USA.

Cause:
Maintenance/replacement TVSS module.

Resolution:
The replacement A, B and C phase module is MA1IMA16 (one for each phase).

Key Words:
TVSS, phase module, A, B and C.
Was this helpful?
What can we do to improve the information ?