Technical FAQs

Ask a Question

What are the replacement copper straps that connect the overload block to the 8911DPSO starters ?

Issue:
What are the replacement copper straps that connect the overload block to the 8911DPSO starters ?

Product Line:
8911DPSO 

Environment:
Maintenance

Cause:
Replacement parts

Resolution:
There are no replacement straps for the 8911DPSO starters, the overloads are riveted to the Contactor portion of the Starter.
An entire new 89011DPSO starter will need to be ordered
 

Was this helpful?
What can we do to improve the information ?