Technical FAQs

Ask a Question

On 8630SFO1PV81Y195, what is the difference between Y195 and Form S.

Issue:  For 8630 RVS, what is the difference between Y195 and Form S.

Product Line:
CLASS 8630, RVS

Environment:  8630

Cause:  Customer needs to determine which form to use.

Resolution: Y195 is all coils to be same voltage and  S is if the only coil at 120V would be the timing relay.

Keywords: Reduced Voltage starters.
Was this helpful?
What can we do to improve the information ?