Technical FAQs

Ask a Question

Are the operators on the 9001SKY201 momentary or maintained?

Issue:
Needs to know if the pushbuttons on the 9001SKY101 are momentary or maintained.

Product Line:
9001SKY201

Environment:
Products sold and used in the United States
 
Resolution:

The SKY201 has the following two operators:

9001SKR1B
9001SKR3R.

Both are momentary.

Was this helpful?
What can we do to improve the information ?