Technical FAQs

Ask a Question

What is the part number for the new SIX, SIP, and SID type isolation, dual voltage, and duplex Medical and hospital panel screws and clips?

 Issue
What is the part number for the new SIX, SIP, and SID type isolation, dual voltage, and duplex Medical and hospital panel screws and clips?

Product Line:
OR Panels/LIM S

Environment:
Maintenance

Cause:
Trim Screws for  medical/hospital isolation panels.

Resolution:
The hardware bag with the trim screws and clips is part number 4800S10200300. This includes enough clips and screws for 1 panel.
 
Was this helpful?
What can we do to improve the information ?