Technical FAQs

Ask a Question

How do you trigger the scope trace in SoMove Lite while the motor is running?

Issue:
Screen displays message "waiting for trigger" after start trace.
Product Line:
SoMove Lite
Environment:
V1.9.4.1
Cause:
Trigger should be set to "Expert" and Type must be set to "Windows in"
Resolution:
See the attached document.
Was this helpful?
What can we do to improve the information ?